Mouser Now Stocking STMicroelectronics' STM32F7 Microcontrollers and Discovery Kit
August 12, 2015 - Mouser Electronics, Inc. is now stocking the STM32F7 series 32-bit microcontrollers and the STM32F746G Discovery Kit from STMicroelectronics (ST). With ST's ART Accelerator™ as well as an L1 cache, ST STM32F7 devices deliver the maximum theoretical performance of the ARM® Cortex®‑M7, whether code is executed from embedded Flash or external memory. The new Discovery Kit provides an easy‑to‑use development platform for the ST STM32F7 series of very high-performance microcontrollers, and comes with the STM32Cube software tool and a full set of demo software libraries for reduced development efforts, time, and cost.
STM32F746 series microcontrollers, available from Mouser Electronics, are based on the ARM® Cortex®‑M7 core with a floating point unit (FPU), which supports all ARM single-precision data-processing instructions and data types. They feature up to 1MByte of Flash, 320KB of SRAM (including 64KB of data TCM RAM), three 12‑bit analog-to-digital converters (ADCs), and two digital-to-analog converters (DACs). Interface options include USART, I2C, SPI/I2S, USB OTG FS, HS, CAN, and SD/MMC.
The STM32F746G Discovery Kit includes an onboard LCD-TFT display with capacitive touch screen and Arduino Uno Rev3 connectors, offering everything required for both beginners and experienced developers to quickly get started developing applications for STM32F7 microcontrollers. The full range of hardware features on the board helps designers to evaluate almost all of the microcontroller's peripherals, including MEMS digital microphones, SPDIF RCA input, and the 4.3‑inch color LCD-TFT screen. The board also features two micro-USB jacks, MicroSD card connector, RJ45 connector, and 3.5mm audio input and output. The integrated ST-LINK/V2-1 via mini-USB connector provides an embedded in-circuit debugger and programmer for the STM32F746 microcontroller. The board also supports software development with ARM mbed.
The features of the STM32F746G Discovery Kit make it ideal for home audio, motor control, security, and Internet of Things (IoT) applications.
To learn more about the 32F746G Discovery Kit and STM32F746 series microcontrollers from Mouser, visit http://www.mouser.com/new/stmicroelectronics/stm-stm32f7-mcu-fpu/.
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 21 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About STMicroelectronics
STMicroelectronics is a global independent semiconductor company and a leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivaled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio, and strategic partners positions, STMicroelectronics is at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence trends.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com