Mouser Now Stocking Crocus XtremeSense CT220, Industry's First TMR Contactless Current Sensors
January 28, 2021 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the CT220 XtremeSense™ contactless current sensors from Crocus Technology.
Crocus CT220 sensors are powered by Crocus' patented XtremeSense tunnel magneto-resistance (TMR) 1D technology, which enables them to detect slight changes in AC or DC current. The sensors offer a 2.7V to 5.5V supply voltage range and 1.2mA supply current rating in a five-lead SOT23 package. CT220 sensors measure the magnetic field of the current flowing through a busbar or printed circuit board (PCB) trace and convert it to an analog output voltage that represents the field and current. These sensors achieve XtremeSense performance with a typical total out error of ±0.5% while sensing field as low as 5mA. Crocus CT220 XtremeSense current sensors feature an inherently high isolation, making them an ideal solution for applications where product safety compliance is a requirement.
Applications for the Crocus CT220 sensors include motor controls, solar inverters, power distribution units and power supplies, and Internet of Things (IoT) devices.
To learn more, visit https://www.mouser.com/new/crocus-technology/crocus-ct220-xtremesense-sensors/.
As a global authorized distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed customers' designs, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Center, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 1,100 manufacturer brands. Mouser offers 27 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 630,000 customers in 223 countries/territories from its 1 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com