Mouser Electronics Empowers the Future of Smart Homes with Online Resource Hub

Do natychmiastowej publikacji

Połącz się z nami


Browse Mouser's smart home resource center
Browse Mouser's smart home resource center

June 26, 2025Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, provides engineers with the latest innovations in automation solutions in its comprehensive smart home resource center. The growing number of Internet of Things (IoT) devices enables the management of the entire home, creating a unique experience for homeowners with greater control, peace of mind, and the potential for long-term cost savings. IoT devices like thermostats, refrigerators, and vacuums offer intelligent automation by learning user preferences and optimizing energy use through real-time data analysis. By integrating internet-connected devices and systems, the smart home, once a futuristic concept, is now a modern reality.

Progress in connectivity, such as tri-radio technology, integrates Wi-Fi® 6, Bluetooth® Low Energy, and IEEE 802.15.4 standard into a single component. This lays the foundation for a modernized network experience, enhancing speed, capacity, and security across IoT devices. When coupled with universal standards like Matter, these technologies create a seamless, interconnected environment where devices communicate effortlessly. This unified IoT system can respond intuitively to real-world conditions, automatically watering plants based on soil conditions or switching on lights when it senses a car in the driveway.

Mouser's smart home content hub offers an extensive collection of articles, blogs, eBooks, and products to help engineering professionals deepen their understanding of automated system design. Curated by technical experts and manufacturing partners, these resources explore how to build a tailored, connected home, including how to harness emerging technologies like Amazon Sidewalk.

Mouser stocks the industry's widest selection of semiconductors and electronic components, including the following products and solutions for smart home applications:

The ABX00112 Nano Matter board by Arduino features the powerful MGM240S microcontroller from Silicon Labs. It seamlessly incorporates the advanced Matter standard for IoT connectivity, catering to hobbyists and professionals. With compact dimensions of 18mm x 45mm, the component is ideal for energy-efficient projects that require connectivity options like Bluetooth Low Energy and OpenThread®, like climate control and environmental monitoring.

The QM45655 front end module (FEM) from Qorvo is developed for Wi-Fi 7 (802.11be) systems. The QM45655 allows for a minimal layout area with integrated matching and a small form factor. The multiple Wi-Fi TX modes on the device optimize output power, linearity, and power dissipation. This conserves power consumption while maintaining the highest linear output power and throughput. The QM45655 is suitable for wearable and smart home applications.

The FRDM i.MX 91 development board by NXP Semiconductors is designed to evaluate i.MX 91 applications processors that allow the rapid creation of Linux®-based edge devices. The development board features a rich set of interfaces, PMIC, and a Tri-Radio Wi-Fi 6, Bluetooth Low Energy, and 802.15.4 module, making it ideal for industrial, automotive, and IoT applications.

The ISM 868/915MHz FPC antennas from TE Connectivity / Linx Technologies are designed for LoRaWAN and IoT applications to address the growing demand for Industrial Scientific and Medical (ISM) antennas with a single frequency. These ISM antennas are available in multiple FPC shapes with double-sided adhesive tape, simplifying mounting within the device, even on curved areas. The ISM 868/915MHz FPC Antennas are optimized for specific frequency bands, depending on product selection, and are suitable for medical devices, home automation, and irrigation control.

To learn more, visit https://resources.mouser.com/smart-home/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Firma Mouser to autoryzowany globalny dystrybutor, który oferuje najszerszy wybór półprzewodników i podzespołów elektronicznych — dostępnych na stanie i gotowych do wysyłki. Klienci firmy Mouser mogą oczekiwać w 100% certyfikowanych, oryginalnych produktów, których pochodzenie od każdego partnera produkcyjnego jest w pełni identyfikowalne. Aby przyśpieszyć pracę klientów nad tworzeniem nowych projektów, witryna firmy Mouser jest wyposażona w obszerną kolekcję zasobów technicznych, m.in. Centrum zasobów technicznych. Ponadto umożliwia dostęp do kart katalogowych produktów, projektów referencyjnych dotyczących poszczególnych dostawców, uwag na temat zastosowań, technicznych informacji o projektach, narzędzi inżynierskich i innych potrzebnych materiałów.

O Mouser

2026 - Firma Mouser Electronics jest autoryzowanym dystrybutorem półprzewodników i podzespołów elektronicznych skoncentrowanym na wprowadzaniu nowych produktów pochodzących od partnerów produkcyjnych. Witryna mouser.com, która służy globalnej społeczności inżynierów elektroników i klientów, jest dostępna w wielu językach, obsługuje wiele walut i oferuje ponad 6,8 miliona produktów od ponad 1200 wytwórców. Firma Mouser ma 28 ośrodków wsparcia na całym świecie, które zapewniają najlepszą w swojej klasie obsługę w lokalnych językach oraz w lokalnej walucie i strefie czasowej. Firma wysyła towary do ponad 650 000 klientów z ponad 223 krajów i terytoriów ze swojego nowoczesnego centrum o powierzchni 93 000 metrów kwadratowych, które znajduje się w obszarze metropolitalnym Dallas w Teksasie. Aby uzyskać więcej informacji, odwiedź witrynę https://www.mouser.com.

Znaki handlowe

Mouser i Mouser Electronics to zarejestrowane znaki handlowe firmy Mouser Electronics, Inc. Wszystkie inne produkty, logotypy i nazwy firm wymienione w niniejszym dokumencie mogą być znakami handlowymi ich właścicieli.

W celu uzyskania dalszych informacji prosimy o kontakt:
Kevin Hess, Mouser Electronics
Starszy Wiceprezes ds. Marketingu
+1 (817) 804-3833
W sprawie zapytań prasowych prosimy o kontakt:
Kelly DeGarmo, Mouser Electronics
Kierownik ds. komunikacji korporacyjnej i relacji z mediami
+1 (817) 804-7764